Hi,
To boot Jacinto 6 EVM board from U-Boot:
1. Connect theJacinto 6 EVM target board to windows host system.
2. On windows host machine, start terminal program with these settings:
Baud: 115200
Bits: 8
Stop bits: 1
Parity: none
3. Connect the Jacinto 6 EVM board to the power supply, then push the PWR RESET button.
But I can't see the output from U-Boot appear on the host system console.
I have copied three image to micro SD card:
ifs-dra74x-vayu-evm.bin MLO u-boot.img
SW2-2 and SW2-3 set to ON.
SW5-1, SW5-3 and SW5-5 set to ON.