Hi,
I am designing a Single phase inverter for PV Applications. The rating is 1KW and i will be using IGBT switches. The switching frequency will be 10KHz. The DC input Voltage will be from 350 to 400 Volts. The ac output voltage will be 230 V. The output frequency will be 50Hz. I am planning to use an LC filter at the inverters output. This i am planning to use in grid connected as well as standalone mode. The grid frequency is 50Hz and grid voltage is 230V . I want some guidance regarding the LC filter design and also about the control strategy.
Hoping for a reply.
With Regards
Unnikrishnan
C K;
For help with your filter design you might try "ELECTRONIC FILTER DESIGN HANDBOOK" Fourth Edition, by Williams and Taylor, published by McGraw-Hill in 2006. It is ISBN 0-07-147171-5
HANDBOOK" Fourth Edition, by Williams and Taylor, published by McGraw-Hill in 2006. It is ISBN 0-07-147171-5
Regards, Neil P. Albaugh ex-Burr-Brown
Thank you
With Regards,
Unnikrishnan C K