Dear All,
In dome, we have two led light source (warm white, 2850 - 3200 degree kelvin). I need to control this light at 31.5 asb constant using PWM technique. I have designed light sensing circuit using OPT101 with 5V power supply, the output is fed to ADC of microcontroller. The mounting of OPT101 is done place which get sufficient light and can be change if needed.
Does any relation between the light out (asb) to current through OPT101 photo diode so that expected voltage can be calculate, scaling of it to feed 3.3V Full Scale range on ADC keeping the same location of opt101 and light source. I like to avoid any external component, like to use the circuit figure 1 (Basic circuit) in its datasheet. Can any comment on it.
One more thing, why output voltage in negative, it must be positive
Thanks in advance
Mahabir Prasad