This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

LMP91200 default Mode setup + problems

Other Parts Discussed in Thread: LMP91200

Hello sir,

we have choosen LMP91200 for PH measurement..here is the sensor details

sensor has 3 pins and it is ISFET based sensor..The reference electrode(AG/Agcl) is inside a glass tube filled with KCL solution.They call it as gate... the other 2 connections are source and drain. it does not need temperature compensation..

it is working well with old design (Discrete IC) and produces (0.865V with ph4 solution, 1.040v with ph7, 1.175v with ph10) ..now we are planning to replace it with LMP91200. we dont need SPI ..just default setup for PH is fine..and also we dont use any connectors directly soldering this wires of sensors..

we tried already with one LMP91200, 0.1uf -- on VCC, 0.1uf -vref. vcc range tried from 2 to 5v.

scl,sdi--gnd

csb,vref--vcc

VCM---- drain of sensor

guard1,2---ref electrode

inp--source of sensor

vout single ended mode with ref to gnd..

tested with multimeter voltage

problem ---vout  variation is very low...(at 3V vcc,vref, vout --(ph4--1.512V, ph7-1.520,ph10-1.532)..and also mostly repeated same values not coming..keeps on varying...so help me out.Thank u