Question #1: Does the TS5A23166 have any known failure modes or weaknesses?
I am using it in a new circuit I am designing. The original breadboard, built on a Radio Shack experimenter's board, works fine. I laid out a supposedly identical 4-layer prototype PC board and see repeated failures. Typically the circuit works for a few minutes or maybe up to an hour, then the TS5A23166 fails for no apparent reason, even when the circuit is just running on the bench, unattended.
The circuit runs at 5Vdc. The original breadboard is powered directly from a 5V lab supply. The prototype PC board includes an LM78L05A regulator to drop 9V to 5V, but most recently I removed the regulator and ran the board directly from the same 5V lab supply. I also added current limiting resistors (a few hundred ohms) around the inputs, outputs and control inputs, but still get failures.
I am searching for differences between the breadboard and prototype circuits but have not found any yet, so I thought I'd post this question. The application is continuous industrial measurement, so reliability is critical.
Question #2: Are there similar analog gates with higher voltage ratings or which might be more rugged? I need response times of a few nanoseconds and "on" resistances of a few ohms. I am not switching power. The signals are under 5Vac at about 100kHz, with currents under 1 mA.
Thank you