After I have configured the HDC1000 in both temp & Humidity conversion mode[Writing 0x1000 in to configuration register(address:0x02)],
1)I am getting 0xFFFC as same value for both temp & Humidity when I am following the below sequence start,address+w,00(pointer register), stop command, wait for DRDYn to be low , start, address+Read.
2)I am not getting the signal DRDYn asserted if stop command is not given after start,address+w,00(pointer register).
Kindly suggest whether stop command need to be given after the Trigger of start temperature & humidity conversion[by attempting writing 0X00 in Pointer register] before giving the read command of both Temperature & Humidity at a time.
Awaiting for your reply soon.
Regards,
N.vamsi.