Hi TI
I would like to use TS3A4751 switch in a product, but i think the datasheet is a bit confusing regarding supply voltages.
The maximum VCC is 4V in the datasheet but the recommended VCC is max 3.3V - So my question is whether 3.67V (lithium cell) operation is actually safe ?
It says that operation above recommended conditions is not implied - based on this 3.67V operations is not safe or ?
Maybe you can clarify difference the actual difference between max ratings and recommended conditions.
Thanks in advance
Br