This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

  • Resolved

DRV8662: Connecting Multiple Haptic Drivers or Multiple Piezo-actuators

Part Number: DRV8662

Hi Kelly,

Sorry I just have a few more questions. Would it be possible to connect multiple DRV8662 to a microcontroller instead of multiple EVMs? If this is possible, could you give us some tips on how it could be done? Or would the connections become too complicated in this case?

Also, I have a reference picture from an article about TI haptic drivers: https://www.electronicsweekly.com/news/products/sensors-products/haptics-redefine-the-machine-human-interface-2015-06/

Would it be possible to connect multiple actuators like the picture shown below? Or are the switches not controlled by a digital source and mechanical instead?

 

Thanks so much for your help! I really appreciate it.

Kate

  • Hi Kate,

    I will look into this and provide a response in the next few days. Sorry for the delayed response.
    I beleive you could do something like this, but I need some time to review this.

    Regards,
    Kelly Griffin
    Application Engineer

  • In reply to Kelly Griffin:

    Hi Kelly,

    Great, thank you so much for your help. Hope to hear back from you soon!

    Kate

  • In reply to Kate Lee:

    Hi Kate,
    Sorry for the delay. Both solutions are possible. You could connect multiple DRV8662 devices to the same microcontroller and then turn the DRV8662 on/off using the Enable pin. This gives the advantage of being able to drive multiple buttons at the same time. The challenges would be determining how to provide the input signals. They could either all be connected to the same input or each IC has individual inputs.
    The other option is to drive multiple actuators with the same driver like the image you attached. This is possible by using high-voltage, low-power FET switches to switch between actuators. We are working on a reference design around this type of circuit. You can use the MCU to turn on/off the gates of the FETs. With this design, you would only be able to drive a single element at a time depending on the piezo capacitance. Our device can only provide ~1W of power.
    I hope this helps and please let me know if you have any additional questions.

    Regards,
    Kelly Griffin
    Application Engineer

This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.