• TI Thinks Resolved

DRV8662EVM: Suggestions for FET switches for connecting multiple actuators

Part Number: DRV8662EVM

Hello,

Hope you are well. I've previously asked about connecting multiple actuators for the DRV8662EVM, and the suggestion was to use FETs to switch between actuators. (https://e2e.ti.com/support/other_analog/haptics/f/927/t/589703)

We've tried to use such method with a 100V MOSFET from Infineon (072N10N), but we're having some difficulties. From what I understand, our issue is that the capacitance is high for MOSFETs, so there is coupling of signals, especially a problem when using FETs for AC signals.

If it's not too much trouble, would it be possible for you to suggest some MOSFETs that are compatible with the DRV8662EVM or other switching methods?

Thank you and hope to hear from you soon.

Kate