We are having an issue with DRV2605s unexpectedly turning on at full strength when the power rail is initialized. The DRV can be completely disconnected from I2C and this will still occur. We have multiple DRV2605s on this power rail, and some have this problem while others do not - some even have it sporadically, and occasionally turn on at startup.
The power rail is operating at 3.6Vdd. We're wondering if this might be happening because the power rail climbs to this voltage too slowly at startup, as there's a note in the DRV2605 datasheet brownout protection section that mentions the device falling into an "unknown state" if the Vdd rise is slower than 3.6kV/s. If this is the case, what can we do to prevent it? Note that if the devices are connected to a table power supply at the same voltage, they do not experience the issue.
Thanks!