Other Parts Discussed in Thread: DRV2624, DRV2625
Hi,
I would like to ask you a following question.
Q) LRA Frequency Range
I have an old datasheet of DRV2605 "SLOS825A" and there describes LRA frequency range (fLRA) is from 50Hz to 300Hz as below (page3).
On the other hand, about the latest datasheet "SLOS825D", the specification is from 125 to 300Hz.
Why did this change (50Hz ---> 125Hz) happen?
It has not already been possible to use 50Hz LRA for DRV2605??
If yes, do you have another solution to drive the LRA whose frequency is under 125Hz?
Thank you for your support.
Best Regards,