This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

DRV8662EVM: Changing waveform frequency and Controlling EVM Modes without pushbutton

Part Number: DRV8662EVM
Other Parts Discussed in Thread: MSP-FET, DRV8662, DRV2667EVM-CT, DRV2667

Hi Kelly,

Hope you're well. I have two questions about the DRV8662EVM. The first is about changing the waveform frequency.  I know that the MSP430 can be reprogrammed to change the waveform, but is there a simpler way to change the frequency? Or do we have to use the full set (Code Composer Studio + JTAG + MSP-FET) connections to alter the frequency?

The second question is about controlling EVM modes. Is there some way we can define the default EVM mode without the pushbutton? For instance, when the EVM is turned on, it is directly set to Mode 6: External Analog/PWM Input.

Hope to hear from you soon. Thank you for your help.

Kate

  • Hi Kate,

    The DRV8662EVM is limited in its capabilities for evaluation. We typically suggest using the DRV2667EVM-CT for evaluation. The DRV2667 contains the DRV8662 and a digital chip with a DAC and RAM memory. So the performance possible with the DRV2667 is also possible with the DRV8662 , but it is much easier to make waveforms for evaluation using our Haptic Control Console program with the DRV2667.

    To achieve either of your questions, you will have to edit the code using CCS and the JTAG connector.

  • Kelly,

    Thank you for your reply. We also purchased the DRV2667EVM-CT, so we will definitely try that one out for our evaluation.

    Just to confirm, does editing the code not require the MSP-FET? Also, similar to my previous question about the DRV8662EVM, can the default mode be changed through the same method for the DRV2667EVM-CT?

    As always, thanks for your help.

    Kate

  • Hi, Kate:

    MSP-FET is used to program the DRV2667 on-board MCU.

    the default mode can be changed with the help of Code Composer Studio and MSP-FET.

  • Hi Peter,

    Thank you for your quick reply. So just to make sure, we need to purchase the MSP-FET, JTAG connection, and download the Code Composer Studio?

    Kate
  • Hi, Kate:

    we are using SPY-wire connection for programming the onboard MCU.

    please refer to below :