This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

DRV2700EVM-HV500: Please suggest the transformer with higher saturation current for DRV2700 HV flyback application

Part Number: DRV2700EVM-HV500
Other Parts Discussed in Thread: DRV2700,


Currently we are using the DRV2700 to drive the piezoactuator as fast as we can. The saturation current of ATB3225, you suggested in HV500 is 0.6A. It is too small for us. Can you help to suggest a transformer with higher saturation current (~2A)?. We hope DRV2700 can have 150V 60mA output capability. Very appreciate your help.