Hello.
I want to ask about DRV8662 input.
Can the DC voltage be applied to the input (IN + / IN -) of the DRV 8662?
If the input contains a bias circuit for AC coupling, is AC input only?
Also, can input variable duty input of DRV 8662 other than duty 50%, for example 10% to 90%?
It is to make the output of the DRV 8662 variable.
Regards.
k-hashi.