We are using the DRV2625 haptic driver and have a question about the initialization procedure. On page 63 of the datasheet, step 3 in the initialization procedure states “Write the MODE parameter (address 0x01) to value 0x00 to remove the device from standby mode.”
I find this statement very confusing since address is 0x01 is a read-only status register (see page 36) and the MODE parameter is in address 0x07 (see page 39).
Can you provide some clarification of this statement?