Other Parts Discussed in Thread: DRV2700
CH1(Yellow) is the input waveform
CH2(Blue) is the output waveform
Because the M430 MCU output square wave ~ ~ is not the frequency I want ~ ~ so I use an external way ~ ~
Received TP7 or TP8.
GAIN0 and GAIN1 setting follow as:
set at 00 the upper and lower weeks will be jitter.
01 half of the week will be shaking
10 half of the week will shake
11 half of the week will shake
The voltage setting is not changed and is maintained at 24V
Input power: USB 5V
Demo board has not changed any parts ~~~
I am currently using the manual way to use this IC, please help me look at where is not set to, or what values I did not change, resulting in output waveform jitter,thanks.