Tool/software: Linux
Dear sirs,
I face a problem. We have a device, and the vibrator on it which control by DRV2624 can not vibrate. The waveform and sequencer configure is right. The vibrator can work on another device(registers setting, software and device are all the same).
The problem device's kernel error is "drv2624_set_go_bit, GO fail, stop action", and the registers writing and reading is running right.
Could you help to analyze the cause of the problem. Is there any way to detect any errors in DRV2624? Whether the state of the register can be read and analyze.
The Address: 0x01, value is 0x04.
Thank you.