Hi team,
Our customer is considering to use DRV2700 in flyback mode.
In order to decide constants and part numbers, please tell me the following points.
#1 Inductor and Rext
It is written to limit the current limit so that the inductor does not saturate in the data sheet.
Looking at the DRV 2700 EVM-HV500, the current limit seems to be set at 1.4A, but the saturation current of the used inductor seems to be 0.6A.
How should we decide the inductor and current limit?
#2 OFF surge protection circuit for SW terminal
In a general flyback circuit, snubber circuits are often seen to protect IC from the negative surge when the SW terminal is OFF.
If the current value and the inductance value satisfy the requirement, since the SW terminal voltage will not exceed absolute maximum voltage, can I think that it is not needed snubber circuit?
Since we want to judge whether or not a snubber circuit is necessary, we want to know whether it is clear that it is not necessary.
#3 Pulldown FET
What kind of rated FET should be chosen when selecting a pull-down FET?
I think that we should choose a product rated higher than the maximum power consumption of FET, but please tell me how to calculate maximum power consumption for FET.
Best regards,
Tomoaki Yoshida