Hi,
I am trying to drive the Powerhap actuator from TDK with the DRV2667
Judging from the datasheets for the powerhap it seems that it cannot be driven negatively, however apparently you tested the same actuator so I am interested in whether or not you drove it differentially anyway.
Assuming you can't I have figured there are two ways in which to drive the actuator single ended using the internal Ram which is essential to my project.
Driving only with direct waveforms ranging between 0x00 and 0x80, this is less ideal for me as driving purely with direct waveforms puts limitations on the 2kb ram, and is also rather time-consuming.
Leaving out- floating and only driving using out+ and driving with Synthesized wave-forms as well, judging from FIG 10 on the datasheet it seems that the sinusoids are generated by two combined differential sinusoids on both outputs rather than say two half-bridge rectified waveforms, is this correct or will the shapes of the individual sinusoids be significantly different with an unbalanced load?
So will leaving one output of the DRV2667 floating, aka an very unbalanced load cause any issues/damage to the DRV2667 (the load of the powerhap actuator in question is 1uf)
Regards,
Rob