Other Parts Discussed in Thread: DRV8662, DRV2665, DRV2667
Hi,
I have been asked to develop a circuit for driving a Piezo Fan Blade with the following spec
Input Voltage: 110±20% V AC
Resonant frequency fr: 50 Hz ±2%
Static capacitance Cs: 17nF±20%@ 120Hz/1V
We want to drive from a DC supply - 12V or 5V.
I was looking at the DRV2700 but wondered whether there might be a better suited part available that could be recommended?
Thanks
Howard