This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

DRV2700EVM: Equivalent of DRV2700EVM for higher frequencies

Part Number: DRV2700EVM
Other Parts Discussed in Thread: , DRV2700

Hello,

We are looking for an amplifier to drive piezoelectric actuators for new application.
Currently, we are using your “Piezo Eval Kit DRV2700EVM” and your “Piezo Eval Kit DRV2700EVM-HV500”. They work perfectly for our current application (output voltages around 200V/300V – PWM frequency of 300Hz – Output capacitive load around 10-15nF).

But for a new application, we need to strongly increase the PWM frequency to about 70KHz, and it seems that the DRV2700 can not support such a high frequency…
In your opinion, which solution would be best suited to our needs? Does it exist any new component which can achieve these specifications (like the DRV2700 chip but with higher input/output frequencies)?

Best Regards.