I have a new DRV2700EVM.
I installed the Piezo Console. I could select "DRV2700EVM" in the Console menu and I get a GUI window marked "DRV2700EVM -- Simulator"
The board did appear in the USB window and if I clicked "connect" the status in the "Connection" box changed to USB-HID. However, the GUI window continued to say "Simulator" and I could not interact with the board.
Then, following forum advice I tried to update the firmware. I guess you have to hold down switch SW1 to get to the boot loader. I did this, but the firmware update process failed as you can see in the screen shot. I think the device is now partially "bricked" as it does not enumerate as any USB device unless I hold down SW1 to get the boot loader back.
Any suggestions?