Dear all,
one of my AA, has found some typos in the DS:
1.
Section 7.4.1 Operation in Shutdown Mode
The NRST pin of the DRV2511-Q1 device puts the device in a shutdown mode. When NRST is asserted (logic low), all internal blocks of the device are off to achieve ultra low power.
The NRST pin does not exist. Are you referring to the EN pin (positive logic) ?
2.
First line (gain 20dB) of Table 1 in the datasheet (section 7.3.1) does not match first line of Table 4 in section 3.4 of User guide of the EVM. Which is the right one ?
3.
Is there any characterization of the RDSON at hot temperature ? At least a rough data.
thanks,
Domenico