Hi Team,
My customer considers to use DRV2667 for their system and studying supply current of DRV2667 now.
I would like to ask abut Figure 8.
1)
Can we estimate supply current value under CLOAD=1600nF?
Another parameters are the same with Figure 8 in this case.
2)
Figure 8 shows supply current is 50mA under 10Vpp, 200Hz.
Can we estimate how much supply current value decrease if we change PVDD from 30V to 25V?
Best Regards,
Yaita / Japan disty