I'm using the DRV2605L to drive an ERM in PWM mode with bidirectional input, and open loop. I'm setting the PWM line to just stay high (100% DC) in order to get the full strength signal. My supply voltage is 3.3V, and plugging OD_CLAMP, DRIVE_TIME, IDISS_TIME, and BLANKING_TIME values into equation 8 V(ERM_CLAMP) should be 3.3V, but the largest output voltage I'm able to get is only ~1.8V.
Is this really the maximum voltage I can get with my setup? If not what settings could I use to get me close to the full 3.3V I'm after?