I was curious of the consequence of adjusting the set resistors to increase the boost voltage above 105V. Will this actually increase the Vpp to over 200V? If used with an analog input, and lower frequency would I be able to get away with this. The load will be driven very infrequently so I don't foresee overheating being much of a concern. Will the Vboost, with the gains at 1,1 even be raised above 105V if the R2 value is adjusted to something like R2 = 8.197kΩ while the R1 value remains at 768kΩ?