This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

DRV2700EVM: pin occupancy for control a signal 0 - 48 V

Part Number: DRV2700EVM

Hello,

i need the correct pin occupancy. 
My external analog signal has an amplitude of 4 V without an offset (-2 V to 2 V). At the output i need 0 V to 48 V. So i need an offset of 24 V and a gain of factor 12.

How i have to set the jumper for my application?

I experiment a lot but when i enable the DC-Offset at Pin TP8 (-IN) the output break down.