Hi,
I'm trying to resolve an issue with a custom circuit board using the DRV8662 chip. The circuit is a replica of the DRV8662 application circuit as well as the Eval board minus the MSP430. The input signal is passed through a 0.1uF 16V X7R 0402 capacitor as shown in the datasheet and Eval kit schematics.
I'm sending an input signal which is a 1-Vpp sine wave, but some reason it appears that the input signal is not passing through the capacitor. I only measure a 1.65V DC on the other side of the capacitor. Any reason why this could happen. The rest of the circuit works, the boost voltage is correct and the gain is correct since If I bypass the capacitor, the circuit seems to work ok.
Can you please suggest why the input signal may not propagate through the input capacitor? Here's the part number of the capacitor I used GCM155R71C104JA55D (Digikey: 490-16433-1-ND)
Your help would be greatly appreciated,
Thank You,