This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

DRV8601: GND Thermal Pad - DRV8601 Haptic Driver

Part Number: DRV8601

I ideally would like to GND the themal pad under this IC as I need it to be able to link a GND plane, in the datasheet it states that it has to be connected to the PCB (of course) but it does not state if it can / should also be connected to GND. My assumption is that it can be optionaly connected to GND but it would be great if some could confirm? Thanks Chris

  • Hi Chris,

    Welcome to e2e.
    The pad under DRV8601 can be connected to GND. This is a thermal pad, so it is recommended to connect it to GND plane as it would be of a relatively big area and thus a good heat sink.

    Best regards,
    -Ivan Salazar
    Applications Engineer - Low Power Audio & Actuators