hello
we use DRV2605L to drive LRA.
If the DRV2605L's VDD is powered from 3V to 4.2V, what is the suggested value of rated Voltage( RATED_VOLTAGE[7:0] bit) and overdrive clamp Voltage( OD_CLAMP[7:0] bit)?
In Equation 5, what is the relationship between VDD, V(LRA-CL_RMS) and rated voltage?
and also VDD and Oeverdrive clamp Voltage?
Automatic-Level Calibration process always fails, how to check and correct it?
Thanks