Interface AFE5808 with TSW1405

Hi,

I am trying to test AFE5808 evm with a TSW1405 board. However I cannot find AFE5808 in the device drop-down menu of HSDCpro as I assume the .ini file for it doesn't exist in the 1405 details folder. Can you please send the corresponding .ini file for TSW1405?

Thanks!

5 Replies

  • Is there any update on this issue? I would really appreciate any help regarding this matter. 

  • Shadi,
    I don't think there exists any ini file for the AFE5808, we will have to generate one. In the meantime, please the ADS528x. I think this is the same format. By the way, the TSW1405 will only support 14 bits, only 12 bits.
    Thanks,Chuck

    Chuck Smyth, Applications Engineering, HealthTech-Imaging

    Please verify post if question is answered.

  • In reply to csmyth:

    Hi Chuck,

    Thanks for your response! I was able to make it work with ADS528x and capture LVDS data. However two changes I had to make was using LSB first in ADC settings and also reversing the order of the channels (1-->8 , 2-->7 etc) to capture correctly.

    Thanks,

    Shadi

  • In reply to Shadi:

    Hi Shadi,

     

    Thanks,

    We will incorporate this into HSDCPro for our 12-bit parts.

     

    Chuck

    Chuck Smyth, Applications Engineering, HealthTech-Imaging

    Please verify post if question is answered.

  • In reply to csmyth:

    Is there any update on this topic? We are trying to integrate AFE5808 and TSW1405.

    We cannot find the device in drop down. It will be great if you can provide the ini file for the same. Also, what should we select in the "Download Firmware" section?