Hello,
Has anyone used these converters? I have just started reading the datasheet in order to produce a feasibility study for an industrial camera. I'm mostly concerned about the external trigger to integration start latency.
Best Regards,
Sergio
Hi Sergio,
This was posted to the wrong forum. Sorry it took a while to find it.
I will post it to the "Imaging AFE" forum, where all the VSPxxxx and AFExxxx devices are supported.
Regards,
Werner
The effect of the TRiG function takes effect on the next MCLK. The precise effect is determined by the settings in the TRIG register, (DEC Address= 33, hex address =21).
It may reset the Line counter, increase the frame counter, or Reset the frame counter depending on the setting of the register.
Note that the active polarity of the TRIG signal is also programmable by register (see Registers DEC address 50 and 51).