This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

  • Resolved

TX-SDK-V2: Pattern length issue(LM96570 of TX-SKD-V2)

Part Number: TX-SDK-V2

Hi Im a graduate school student in Korea.

I have a problem with the pattern length of tx-sdk-v2. I am conducting research related to ultrasound stimulation. So we are examining each channel at the same time, and the important issue is the pulse length. My system has a frequency of 2MHz, but the included software has a problem of whether the pattern length is 64, which can send a total of 32 cycles, but can not be increased anymore. At present, 2MHz, 32cycle, the actual time of the ultrasonic irradiation is 16us maximum, but I wonder if there is a way to increase it in milliseconds. I will wait for a good answer.

This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.