hello,
when i run the apllication,folloeing statement is executed
[ 258.526519] --------------------->ISP---- is 6000000[ 258.531585] isp_buf_queue 1535 [ 258.587280] isp_buf_process 1439
.
it takes some 40 t0 50 sec after this statement
[ 258.590698] --------------------->ISP---- is 8000000[ 258.595794] isp_buf_process 1443 [ 258.620605] isp_buf_process 1439 [ 258.624023] --------------------->ISP---- is a000000[ 258.629119] isp_buf_process 1443 [ 258.653900] isp_buf_process 1439 [ 287.927246] isp_buf_queue 1533 [ 287.930511] --------------------->ISP---- is 6000000[ 287.935577] isp_buf_queue 1535 [ 287.942596] isp_buf_process 1439 [ 316.189025] isp_buf_queue 1533 [ 316.192291] --------------------->ISP---- is 8000000[ 316.197357] isp_buf_queue 1535 [ 316.228759] isp_buf_process 1439 [ 345.323059] isp_buf_queue 1533 [ 345.326324] --------------------->ISP---- is a000000[ 345.331390] isp_buf_queue 1535 [ 345.349365] isp_buf_process 1439 [ 374.410064] isp_buf_queue 1533 [ 374.413330] --------------------->ISP---- is 6000000[ 374.418395] isp_buf_queue 1535 [ 374.436676] isp_buf_process 1439 [ 402.456451] isp_buf_queue 1533 [ 402.459716] --------------------->ISP---- is 8000000
this s happening while capturing image...but --------------------->ISP---- is 6000000 this takes nearly 40sec to continue next buffer 8000000..there is much delay in dequeing buffer...so am not able to get any image in file.its just pink color,.
-I am capturing image and storing it in one file.
-am using ov7725 camera,omap3530 processor
-video0 node is getting created..
plz anyone suggest me wat might be the issue
regards,
suzan