Hi,
I'm using AFE8085 and TSW1250 boards for my project. Before i can initiate my project i have 1 doubt. If i'm supplying a 20mVpp sinusoidal signal in any of the channel in AFE5805 and capture the deserialized format in TSW1250 GUI will the same signal (20mVpp sinewave) will be reproduced in the GUI screen.
Thanks & Regards
JITHESH-AR
AFE5805 is a VGA. it is 20dB LNA+-46dB ATT+20~30dB PGA>
thus the min gain is -6dB. the max gain is 50 dB. so it is possible you supply 20mVPp and get 10mVpp out. please read the datasheet plots of Gain vs Vcntl.
THanks!
Is there any minimum limit in frequency that can be applied to AFE5805???..