Hi everyone,
I want to use an AFE5804 in an ultrasonic visualisation project so i bought an evaluation module to do some testing.
My plan is to use an FPGA to capture the serial data from the AFE5804 and deserialize it. For this i would like to use the 40Mhz clock from the AFE5804 to drive the FPGA.
But when i measure the clock (LCLK) from the AFE5804 it is not wat I expected, The duty cycle is no where neare 50% and the frequency is only 400Hz and not constant.
I measure directly on the connector whit a scope (1GHz, 4GSa/s) a screen capture is added. The FCLK lies around 4000Hz.
If somoene can point me in the right direction i'd be very grateful.
Hans Blockx