This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hi,
Please some body who knows about Tx_sdk_v1 powering answer to my questions. It is usefull and urgent for me.
thank you.
regards,
chandu.
Hi Chandu,
Sorry for the late response. I was on vacation.
1) If J_SUB pin is at 1-2 position, you should power up -50V, 3.3V, 1.8V, +/-10V, and then +50V.
2) Technically yes. But we should recommend when the LM96551 outputs are connected to the transducer since the output can overshoot the +/-50V supply by 10% or so; i.e., the output voltage can be at -55V even if VNN is at -50V.
3) If you want to outputs to be at 15V or 20V, then just apply 15V to 20V to VPP & |VNN|.
4) Yes, you can apply a 3.3V to the TX_SDK board and the then click on connect button.
I hope I answer you questions clearly.
Regards,
Charles
Hi sir,
Thanks for valuable information.
If you don't mind let me confirm again about the 4th answer in last reply.
By giving single 3.3v to the Tx solution board Is it possible to GUI connected to the board.
thank you very much sir.
regards,
chandu.
Hi Chandu,
Yes, you can communicated the Opal Kelly board with the TX_SDK board.
Regards,
Charles