Hi
I have a issue.
Please give me a advice.
[Issue]
My customer is using VSP8133.
Rarely, it becomes a frame brighter than other frames since output pulse is floating.
[My reasoning]
I suppose that a coarse adjustment of the Black-Level clamping is performed at the head of the frame.
I suppose that when VSP8133 resived a noise from external at adjusting the Black-Level clamping,
it's occuered the above issue.
[Question]
Q1:At which pin should the measure against a noise be taken?
AVDD? or another? Please give me a advice.
Q2:Please suggest an example layout for the measure against a noise?
The information on the product similar to VSP8133 is also available if it becomes helpful.
Best regards
Shimizu