Hi,
We've connected these two evaluation modules, installed LabView 7.1, then installed the required software for these two modules.
We are using the onboard 40MHz clock. Therefore, we shortened jumpers according to figure 4 on page 5 of "User's Guide SLOU222B–March 2008–Revised November".
It now (after a long series of tries) can acquire new signals when we click on "Capture" button, but we get only noise.
We use a 2MHz pulse generator, but can not recognize any peak at that frequency.
We use only one channel (CH 1) from AFE5805EVM .
Our settings for the "TI ADC SPI interface " are:
ADC: Address byte: 46, Data bytes: 8208, "power down" is "off" only for CH 1. "LOW FREQ. NOISE SUPP" is "on" only for CH 1. "Gain" is 12 for ch 1 and 0 for all other channels.
VCA: THE BUTTONS ARE SHOWING : power on, TGC, BP filter 15MHz, no clamp, PGA gain 30 dB,
Our settings for the "TSW 1250 GUI " are: AFE5805, CHANNEL 1, Hanning, ADC sampling rate 40 MHz, ADC input freq 2MHz, FFT record length 65536.
Our wonder why we just get noise. Anything is missing? What?
The tables and figures are not consistent. It is very hard to know for example which jumper we should short when we get the message "jumper settings for rev B: JP2 = short 1-2, JP8=SHORT 1-2, JP9= SHORT 1-2"
We spent a lot of time on just trying to make it work properly. The information provided by the two pdf-documents is not enough.
We need assistance ASAP.
Thanks in advance,
Satya