The LM96511 data manual says the sampling rate has to be between 40 and 40.5 MSPS. Can it run slower?
I need to simultaneously sample all 8 channels for 8 milliseconds, and I can't find a way to buffer that much data that fast.
I've looked at: Wavevision 5 which only does 2 channels at once; TSW1405EVM appears to do simultaneous 8 channels, but only 64K samples total; National Instruments PXI-6562 appears to only go up to 400Mbps / channel, but 40MSPS from the 12 bit LM96511 would be 480Mbps / channel.
Has anyone found an off-the-shelf way to grab that much LVDS data at those rates?