Hi,
I recently have ordered TSW1405 but realised that it is not compatable with AFE5804 ( Such a silly error)
Is there a connector which is available or which I can buy to connect those two?
I can also make my own connector , if i know the corresponding mating connectors.
Also I am planning to use the AFE 5804 with an FPGA.
What type of connector does it need to connect to an FPGA. I am planing to use Lattice FPGA EPC3 ( Versa Dev kit), the same one used in TSW1405.
Name of component on AFE5804 -
HEADER,SMT,80P,0.5mm,FEM,DIFF
PAIR,RECEPTACLE,168H
Name of Component on TSW1405 -
QSH-060-01-L-D-A-R-T1