Hi everyone,
maybe I am just being blind, but I am trying to interface our AFE5809EVM board which is connected to a TSW1400EVM board via USB.
I can use the GUI that is provided by TI to setup the AFE5809EVM, however, I would like to do so using Matlab instead of the GUI. The board connects as a serial port on my PC, so I assume that the GUI send's it's command using the serial port as well and hence there should be in principle no problem to do the same with Matlab. However, I can't find anything related to doing so on the web.
Any ideas where to find information about automating the AFE5809EVM? Documentation of the serial commands, dlls to use, anything?
Thanks a lot,
Joe