Hi,
I am working with AFE 5809 and try it to configure it through FPGA. I am able to configure IC so that it sends custom patterns. I verified the custom patters using chipscope. But when I am trying to receive continuous echos through a AFE, it does not work properly. I am not able to figure it out what is going wrong while configuring AFE. The configuration data is attached. First 8 bits from MSB are address bits and remaining 16 bit are data bits.
AFE configuration data.txt
0000_0000_0000_0000_0000_0001 0000_0000_0000_0000_0000_0000 0000_0001_0010_0000_0000_0000 0000_0010_0000_0000_0000_0000 0000_0011_1000_0000_0000_0000 0000_0100_0000_0000_0000_0000 0000_0101_0000_0010_1010_1010 0000_1010_0000_0001_0000_0000 0000_1101_0000_0000_0000_0000 0000_1111_0000_0000_0000_0000 0001_0001_0000_0000_0000_0000 0001_0011_0000_0000_0000_0000 0001_0101_0000_0000_0000_0000 0001_0110_0000_0000_0000_0001 0001_1001_0000_0000_0000_0000 0001_1011_0000_0000_0000_0000 0001_1101_0000_0000_0000_0000 0001_1111_0000_0000_0000_0000 0010_0001_0000_0000_0000_0000 0011_0011_0000_0000_0000_0000 0011_0100_0000_0000_0000_0000 0011_0101_0000_0000_0000_0000 0011_0110_0000_0000_0000_0000 0011_0111_0000_0000_0000_0000 0011_1000_0000_0000_0000_0000 0011_1001_0000_0000_0000_0000 0011_1010_0000_0000_0000_0000 0011_1011_0000_0000_0000_0000 0011_1101_0000_0000_0000_0000