Hi everyone,
we are currently developing an Application using 4 of the LM98725. From our first tests we saw that the AFE is getting a bit hot.
We measured TC 80°C (at the case) when running at approximately 35MSPS.
Currently we also have TA 25°C with case open using TTL Outputs. In the real Application TA might rise up to 60°C or still higher, but we can manage that.
What we are really afraid of, is using the LM98725 at 80MSPS, still when the case is open, since then the Case Temperature will rise much more than up to 80°C. My collegue is arguing that we might be actually 10°C above maximum Temperature since in the Datasheet TA is 70°C max. But i believe that in the Datasheet TA is not meaning TC, as well as RJA = RJC + RCA.
We are not using strong drivers at all, since all sensor signals are buffered.
So i also do not believe that we are overloading the LM98725 itself, but the TSSOP Case is just bad in terms of thermal performance and TC is really close to TJ, maybe due to some special packaging?
It would be nice if someone could confirm this thermal behaviour of the LM98725 AFE.
Thanks,
BR Christian