Hi Team,
I have a question about TMP112.
It seems that accuracy of 0℃ to +65℃ is "-0.5℃~+0.5℃" in Electrical Characteristcs.
On the other hand, Figure3 shows that accuracy of 0℃ to +65℃ is "-0.5℃~+0.4℃".
Best Regards,
Yaita / japan disty
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Note: Multiple posts of the same question by one person. We are addressing this on another post.