Hello,
There is the +/-3°C as caluculate maximum object temperature In the TMP006 datasheet at one of the condition.
Could you please let me know the value of "calculate object temperature" when we use TMP006 at the following conditions?
Ta=0°C~45°C
FOV:0°
Distance: 1mm(distance between TMP006 and object is lenz only)
Best Regards,
Ryuji