Hi,
I have a system with TSC2046 controller for a 2.8" TFT (DT028ATFT-TS). The touch screen is a 4 wire one with 300ohms for X and 600 ohms for Y.
The analog connections are short, about 1/2 inch, and the touch controller is decoupled locally with 2.2u and 0.1u.
I experience noise, about 100-200 digital units, when TFT is on. The touch readings are fine when TFT is not initialized. The backlight driver is not adding significant noise to the touch screen readings.
SW: emWin ADS7846 touch driver., with PENIRQ detection, but no BUSY line.
Not sure what to do next, maybe to add input capacitors? I would still try to fix the issue on the HW level before filtering this noise.
Any suggestions, please?
Thank you,
Gabi