Hi,
I am interfacing ADS7843 (TOUCH SCREEN CONTROLLER) with Waveshare electronics 4.3 inch LCD (480x272) & AM335x custom board, with linux running.
But i am unable to understand what platform data should i pass in the "struct ads7846_platform_data".
for example :
the platform data for LCD panel TX09D70VM1CCA (240x320) is
static struct ads7846_platform_data ads_info = {
.model = 7843,
.x_min = 150,
.x_max = 3830,
.y_min = 190,
.y_max = 3830,
.vref_delay_usecs = 100,
.x_plate_ohms = 450,
.y_plate_ohms = 250,
.pressure_max = 15000,
.debounce_max = 1,
.debounce_rep = 0,
.debounce_tol = (~0),
....
};
I need help on how should i calculate the above values using my LCD..!
regards
Nitesh