Hi,
I would like to ask you a question about PENIRQ of TSC2007.
My customer has been evaluationg TSC2007 and found the problem with PENIRQ behavior.
Q) After power-on, following phenomenon has happened.
The PENIRQ signal status keeps "LOW" level under any conditon of X+ (High/Low).
This phenomenon seems to have happened easily on higher temperature. (around 60℃)
Sorry I have not confirmed TSC2007 POR condition of the customer circuits.
But can I understand that this phenomenon is due to POR issue?
Could you tell me any other possible root cause if you know?
Why is it easily happend under high temperature?
Probably in case of using TSC2017, such kind of phenomenon will not appear in same customer circuits.
Is it possible to replace TSC2007 to TSC2017?
Thank you very much in advance.
Best Regards,