Hello Guys,
One of our customers is evaluating TSC2013-Q1 using TSC2013 EVM for the next their product which will be released to market within this year.
They confirm that TSC2013 worked well with the bundled touch panel to TSC2013 EVM.
After that, they checked TSC2013 working with 2 type of other touch panel they had.
Then they found the following problems.
1. Zoom-in/out function work well. But Flick function doesn't work. Do you think what the problem cause is?
If any parameter is adjusted, the flick function works well?
2. They want to know the specification or datasheet of the bundled touch panel to TSC2013 EVM. Do you have it?
And is it a standard parts Or custom part? Is there any special spec on the panel.
3. Can the EVM touch panel sensing level be adjusted or trimmed?
4. They want to know how to detect gestures. Can TSC2013 detect any gesture itself?
Or main CPU connected to TSC2013 need to detect gestures?
The customer wants to decide whether they adopt TSC2013 or not next week.
So they need the answers ASAP. If they can not get the answers, they will adopt the competitor touch panel controller they current using.
We are aiming to replace the current competitor IC with TSC2013. I hope quick answers the questions.
Best regards,
Kazuya Nakai